This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC5928: unused output terminals

Part Number: TLC5928


Hello!

My customer wants to use only 8ch of TLC5928.
(This IC has 16ch OUT terminal)
What should I do with the terminals of the remaining unused channels?

I am concerned about the following two problems.
・ LED open detection
 I think LED open detection works.
 Does it malfunction unless the remaining unused channels are enabled?
・ Constant current output
∙  The OUT terminal is a constant current output, but is it possible to break down the IC even if it is open?

Regards

Hashi