Other Parts Discussed in Thread: BQ25570
Hi, I'm not having success using the EVM with a source that produces about 295mV DC constantly at up to 20uA. However, if I apply 350mV or greater (at around the same current) into VIN_DC via different source, I notice some pulsing (using a DSO) at TP2 (LBOOST) and a step-up in voltage across C6 (CBAT). Below this, no activity is seen at LBOOST. Jumpers are set as in Figure 11 in the User's Guide. Changing VOC_SAMP from 80% to 50% doesn't make any difference. Also, I haven't made any modifications (e.g. changing resistors) on the board. I chose this EVM as it seemed to be the only one with a VIN_DC rating as low as 130mV, however I'm now starting to suspect this could be an error. Any help would be much appreciated. I do have facilities and skill to rework the SMD components onboard. Thanks, Danny.