We have this EVM unit, TPS2373-4EVM-758, on hand.
We connected the EVM input to a DC Power Supply. EVM Output is not connected to any load. As soon we apply input from 0V and gradually increase towards 1V, the input current drawn shoots up suddenly, towards 2A. We switched off the input instantaneously at this point of time, foreseeing any damage to the EVM. We repeated this and got the same result, means no additional damage occurred to the EVM due to our powering up exercise. We did not try with POE PSE, in order to avoid possible damage to the EVM.
How to proceed?