This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2060A: Cant communicate to EV2200 on windows 7 system

Part Number: BQ2060A
Other Parts Discussed in Thread: BQ2060, , EV2400, BQ4050

Hello,

I have an EV2200 and the EV2200-60 software installed.  My VSS is connected to pack- of my bq2060A.  I have a USB to RS232 FTDI converter installed and it is recognized as COM4 on my PC.  I cant seem to establish communication with the EV2200 nor my bq2060a.  I try to force communication on COM4 and it fails.  I jump started the pack and can see the pack voltage on the output so i know the bq2060 is active.  Am i missing a driver for the EV2200?  Can someone point me to where it is if that is the case?

Thank you in advance.