This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561: Facing issue with garbage data

Part Number: BQ27Z561


Kang,

Pls. go through the link on which customer has posted the query.

https://e2e.ti.com/support/power-management/f/196/t/849391?tisearch=e2e-sitesearch&keymatch=BQ27Z561

As you have suggested they are reading more than twice in a second. Still they are facing the issue with garbage value & random in nature. When they reads registers twice in a second, during 24 hours they are getting garbage value almost 15 to 20 times. 

When they speedup the readings/ second then they observed more garbage & on slowing down no. of garbage values are less. Looks like device is throwing garbage values for same no. of times for lower speed or higher speed for sample size of 50K or 100K or whatever the numbers are.

kindly help resolving the issue. Also we are not able to understand even if we will read at higher speed why device is giving garbage, at the most it should throw same data.

Mitesh