This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The BQ27541-V200 fuel gauge is used inside Li-Ion battery. In my application, I need to use two similar batteries in series.
After the series connection of batteries, I am able to read I2C of second battery whose GND is connected to the Board. NOT able to read I2C of first battery.
I understand that as the GND of first battery is connected VBAT of second battery the reference of first one is shifted to VBAT. How to resolve this.
Thanks,
Kaliga.
hi Kaliga
You can't use two of these gauge in series. It is not designed to function that way. if you need a 2s gauge, consider the bq28z610
thanks
Onyx