Other Parts Discussed in Thread: BQ25892
We currently use the BQ25121 and the BQ25892 in our designs.
We now need a charge IC that can handle the following characteristics.
A battery charger to charge a LiPo battery of 630 mAh, charge current 630 mA, cut off current 6.3 mA
I²C access to control and monitor charge.
It should be able to handle a load of 1000 mA.
The BQ25121 does not have enough load capacity.
And the BQ25892 is for larger capacity batteries.
BQ25892 |