Dear Sir,
Our Customer is asking about the PG spec of TPS62135. here is the parameters about PG signal as below.
for the PG signal failing(% of Vout) spec, the Min. is only 3% which it might be reached the spec when RD is doing the transient test. Therefore, could you kinldy let us check if this spec is correct? or is there there min timing for Voutto drop 3% of Vout in order to trigger the PG signal to be low?
above, please kinldy help us check with this and if there is any question, please let me know
Cheers
Alec