Part Number: TPS23754
Other Parts Discussed in Thread: PMP6812,
To whom may it concern.
Hi, I'm HS.
I've got TPS23754EVM - 383. Now I want to use it with flyback.
I happened to find the reference called PMP6812 - Class 4, Cost-optimized, Flyback Converter Reference Design for PoE Applications.
But its efficiency is quite worse than I expected and I assume because now it's quite outdated..?
So I hope I can boost the efficiency using sorta new or better components such as replacing old school diode rectifier with ideal diode bridge(MOSFET) or something like that.
To sum up, My questions are...
1. Can I boost the efficiency of PMP6812 by replacing some components? (Hopefully 90% or higher)
2. If it's quite tricky....are there any TPS23754 reference design for PoE at using flyback(V_OUT=12V) ??
3. What's the biggest difference or kinda criterion when you choose DCDC - Flyback VS Forward ?
4. The schematic of PMP6812 is quite confusing...esp because of the triangle marks.
4-1. What's the purpose of R5, C15, D12??
4-2. Would you break down the Transformer part for me? Especially triangle marks..
5. I'm having a hard time understanding T2P section in PMP6812..esp secondary side.
Would you explain RCs on secondary side? Such as R17, R14, R15, R18, R19, C25, C26, C28 and so on??
Also, There is 0 Ohm resistor, R13. What's the purpose of this 0 Ohm?
Thank you for your hard work and I appreciate it a lot!
Hope you have a good day!