I am using the TPS70102PWP regulator in a design and wanted to know where I should connect the pad. Is this supposed to be left unconnected or shorted to GND?
Also, for this part I want an output voltage of 1.22V, which is the internal reference voltage. Can you confirm that I should connect FB1 to VOUT1 to do this and will not need an external resistor connected between FB1 and GND? Thanks for your help