Part Number: REF102
Other Parts Discussed in Thread: OPA227, , OPA277
Dear member of this forum,
I need to generate a very precise 10 uA current .
I used the schematic in the description of the REF102 chip together with the OPA227 Op Amp.
Additional to the schematic I also supplied the Op Amp ( V+ Pin of Op Amp ) with 12V. As ground for the whole circuit I used the V- Pin of the Op Amp (for measuring the resulting current too).
Please see the schematic I attached to this post.
Here is the issue : When the Op Amp is supplied with voltage the voltage on the resistor falls from the expected 10V to 1.5V. Also the Op Amp gets hot !
I checked the breadboard for short circuits. I also checked for mistakes. On YouTube there is a tutorial with the exact same setup and there it did work !
Still... I used a SOIC Package OPA227 together with an adapter to use it on a breadboard. Maybe is the SOIC Package too sensitive to 12V ?
Any suggestion would be highly appreciated !
Thank you for your time and I am looking forward for your answers !