Other Parts Discussed in Thread: UCC28951
Dear support member.
The customer is mass producing UCC28950.
This project is Urgent.
IC is broken and I have a question.
(Situation)
There is no disturbance in the waveform between OUTA and OUTB.
However, in the waveform between OUTC and OUTD, there is a part where Duty 50% is not continuous and is flying.
(Question)
Q1.
Is the IC abnormal when the waveform is not continuous?
Q2.
If the IC is abnormal, what can be the cause?
I attached waveform.
Could you check it?
Best regard.
Bob Lee.