Part Number: UCC27211
I am adoperating 2 UCC27211 gate driver in a DCDC current controller, the LI and HI inputs are fed by the outputs of a LT3741 controller and LO HO outputs are driving 4 IRL60B216 as it can be seen in this attachment
the inputs of the gate drivers are correctly driven but their outputs are not, the same error can be seen in both drivers
LI and LO:
HI and HO:
Light blue waveforms are the inputs of the UCC and violet waveforms are taken directly at the MOSFET's gates
Speaking about the Low side, i wondered about some voltage drop due to high driver current on the little resistances in series with the gate and i actually noticed that probing directly at the output of the driver
the square wave reaches like 10V (NOT 12V as it should be!!!); hence i tried to modify the value of the resistances but with poor results, i actually also tried to place a 0ohm instead so as to avoid the voltage drop but all I obtained was that 6V square wave clearly both at the gate and at the output of the drivers
Speaking about the High side i wondered about a bad choice of the bootstrap C value, i increased it till 800nF but nothing changed
I also tried to increase the bypass capacitor value up to 4,7uF, to remove the SMDJ15CA and to place a resistor between MOSFET's gates and ground/HS, but still no result! So up to now i have no idea what to do
There is clearly some error in my design because i already used those drivers in a similar design with the same current controller but with different mosfets