This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61220: TLV61220 output problem(Iout 20ma+)

Part Number: TLV61220

HI TI,

In my project, there is a problem in the test.

VIN=4.0V;I_IN=1.64ma;VOUT=5.33;I_OUT=1.1ma;The load is a 5K RES. Efficiency=90%. i think it's good .

when I_out @ (1~10)ma,the VOUT & Efficiency i think no problem.

when I_out @ 20+ma. the VOUT Being lowered, only 4V.and Inductance has noise.

The following PCB is the layout of the reference documentation and EVM.

the waveform of SW(What should be the frequency under normal conditions?). 

CAP(X5R_1206_10uF)

RES(1%_0805)

inductance(4.7uH_30%_1A)

I want to know why this is happening.pls help me~~~