I'm interested in using the BQ24650 to drive a buck converter, but instead of directly using MOSFETs, I want to have it drive a half-bridge circuit (EPC9201) that has low- and high-side signal inputs. The high-side driver signal is referenced to ground in the half-bridge circuit, but the BQ24650 has a level shifter on the high-side driver. Can the BQ24650 high-side driver be referenced to ground (e.g. PH pin to ground, BTST pin to 5 V) so that these two circuits could be used together? Thanks.