This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BQ40Z60: What is temperature error when using mismatching R/T table and coef parameters?

Part Number: BQ40Z60

Tool/software: Code Composer Studio

Thanks Onyx! But you may misunderstand my question. I post again!

1, I understand when I enter R/T table to G4-G35, cell C30 to C34 and cell E30 to E33 coef will follow to change. At the same time graphs 3 and 4 show the temperature error.

But what I want to know is temperature error when using R/T tables of below two sources(NTC 'DHT0A103F34D2SY' , 'JDR103F344F') and below coef(not one based on R/T tables)? In other words, what is the temperature error when using mismatching R/T table and coef? Could you help analyze and give me an answer?

7384.R_T tables for two sources.xlsx

0285.RT1-DHT0A103F34D2SY.PDF

5432.RT1-JDR103F344F.PDF

Calibration

Cell Temperature Model

Coeff a1

-11130

Calibration

Cell Temperature Model

Coeff a2

19142

Calibration

Cell Temperature Model

Coeff a3

-19262

Calibration

Cell Temperature Model

Coeff a4

28203

Calibration

Cell Temperature Model

Coeff a5

892

Calibration

Cell Temperature Model

Coeff b1

328

Calibration

Cell Temperature Model

Coeff b2

-605

Calibration

Cell Temperature Model

Coeff b3

-2443

Calibration

Cell Temperature Model

Coeff b4

4696

Calibration

Cell Temperature Model

Rc0

11703

Calibration

Cell Temperature Model

Adc0

11703

Calibration

Cell Temperature Model

Rpad

0

Calibration

Cell Temperature Model

Rint

0