This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC5957: Daisy Chain Configuration

Expert 4486 points
Part Number: TLC5957

Any input is much appreciated! 

1. Is there example code for any of the following that will be applicable when using a daisy chain configuration besides what is described in the app note SLVUAF0?   

        a.  - example setting the FC register

        b.  - example sending brightness data

        c.  - example reading LOD for each controller  

        d. - example sending GS data for each controller.

 

2. When you set the FC register on a daisy-chain of controllers, do all controllers get set with that one message or do you need to send the message to each controller?

 

3. The app note references (in 3.7.1) "the current operating line" and "total line number". What are these referring to?

Thanks,

Jack