Part Number: TPS54232
Hi,
I am using TPS54232 for generating 5V and 3.3V power supply from Vin = 24V.
I am facing the output supply issue with 5V when giving Vin > 15V. As I increases Vin > 15V, Output and Input nets are getting short with 0.7Ohm resistance only and difference between Vin and Vout is ~2V only.
Till Vin = 15V, IC is generating 5V properly and the strange thing is that I never faced the same issue with Vout = 3.3V. I am only facing this issue with Vout = 5V.
Kindly provide the resolution at the earliest.