Datasheet states that if LEDs are not used DISP pin should be pulled to GND. If the display function is disabled in FW configuration could the DISP pin be left floating?
Couldn't see the DISP pin connection from the pin equivalent diagram on the datasheet. Is there any risk if DISP pin is left floating when the display feature is disabled from the FW?