Hello;
I need to understand whether I should change my design to use the circuit shown on the left side of Figure 13 in slua749a "Figure 13. bq76920 REGSRC Power Option" in the event of a short circuit. I've designed in the circuit on the right side, which separates BAT and REGSRC. Since in this circuit the diode protects REGSRC from a sudden voltage drop due to a short circuit, but BAT is not protected. Does the BAT input also need protection? I had assumed that the 920's HW short circuit comparator would disable the discharge FET within 35-105us, and since these are powered from REGOUT, BAT would not require protection??
Thanks