Other Parts Discussed in Thread: BQ76PL455A-Q1
Tool/software: Code Composer Studio
Hello
How can I program microprocesser in BQ76PL455EVM ? I want to change codes of the EVM and try my own algorithm on the board ? I could not see any pin to connect microcprocessor on board in datasheet ? Actually J3 seems to be right connector but I could not be sure whether I can program it via J3 or not? If I can, what can be pinout of the USB ?
To sum up , I will connect with USB by using CCS and try to implement my own code.
1. Can I do that?
2. Which connectors should I use on board ? Can you share me the pinout ?
3. Does USB fits for that ?
4. Do I need any JTAG component or can I directly connect USB to the J3 ?
Thanks.