This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BQ76PL455EVM: BQ76PL455EVM Programming Pin

Part Number: BQ76PL455EVM
Other Parts Discussed in Thread: BQ76PL455A-Q1

Tool/software: Code Composer Studio

Hello

How can I program microprocesser in BQ76PL455EVM ? I want to change codes of the EVM and try my own algorithm on the board ? I could not see any pin to connect microcprocessor on board in datasheet ? Actually J3 seems to be right connector but I could not be sure whether I can program it via J3 or not? If I can, what can be pinout of the USB ? 

To sum up , I will connect with USB by using CCS and try to implement my own code. 

1. Can I do that? 

2. Which connectors should I use on board ? Can you share me the pinout ?

3. Does USB fits for that ?

4. Do I need any JTAG component or can I directly connect USB to the J3 ?

Thanks.