This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80EVM-020: SMBus communication without the use of an EV2400.

Part Number: BQ40Z80EVM-020
Other Parts Discussed in Thread: BQ40Z80, , EV2400

Hello,

I recently bought a BQ40Z80EVM-020 to help with developing a monitor that will use the bq40z80. I would like to test my host controller and its code on the BQ40Z80EVM-020, but I am not having success communicating with it.

The EVM communicates perfectly with the EV2400, so I am curious if I can only communicate with the EVM with the use of an EV2400.

Is there a configuration that allows a for an alternate SMBus host to issue commands to the BQ40Z80EVM-020?

Thank you,
Joe