This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z655-R1: bq20z65-R1 Max Erro > 100%

Part Number: BQ20Z655-R1

I have a battery that, based on SMBUS and Flash data, should be working properly. However, it is asking for a conditioning cycle. The only oddity I found is that the Max Error is at 144%. All other SMBUS data looks to be appropriate, and Flash data appears to match the golden file except, of course, for the locations that are updated by the processor during cycling. Update status is at 0E, and Ra_Tables appear to be ok. Current, voltage and temperature calibration appear to be ok as well. Any thoughts?