This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24193: How should we set PSEL and OTG?

Part Number: BQ24193

Hi,

There is the PSEL pin that is described as the power source selection input. As of now we are considering to have both PSEL and OTG grounded.

1) Does this input (PSEL high or low) affect anything else than the input current (being 3A or 100mA/500mA)?

2) It is shown in the datasheet that PSEL can be connected directly to ground. To achieve high state instead, can it be connected directly to 3.3V (without pull-up resistor)?

3) My source is 12V/500mA. I will not be using the boost mode (OTG). What PSEL/OTG setup would you suggest? I was considering PSEL low since it is similar to a 12V adapter and simple to implement, yet the current limit is more similar to a USB host. The option to PSEL/OTG = low/low I was thinking of was high/high, if so hopefully without additional component (hence question #2).

Thanks!