Other Parts Discussed in Thread: TPS2663
Hi
My customer has solutions for surge issue,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rakesh:
The LM5060 is used on the output side of the power supply(DC/DC 24 to 48V ),
as need to pass surge test,
when test surge, LM5060 will damage in Sense and Out pin,
my customer put 0.1uF in front of the sense and out pin,
I don't know if this is feasible.
Hi Rakesh:
There is something wrong with the information I have provided to you.
I correct the DC/DC converter input and output information,
input is 18V~32V, output is 24V
output current is 5.42A,OCP is 6.5A, SCP is 8A.
Hi Bryan,
TPS2663 is the right solution for this application. Please have a look and let me know if you have any questions.
Best Regards, Rakesh