How to connect SS/TR pin when my customer will not use Slow start function of TPS54319?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to connect SS/TR pin when my customer will not use Slow start function of TPS54319?
To start as quickly as possible, leave the SS pin unconnected (floating).
MAKE ABSOLUTELY SURE THAT YOUR CUSTOMER TESTS THIS CONFIGURATION ON THE EVM BEFORE GOING TO PRODUCTION. If any converter starts without soft-start, there is the risk of crashing the input bus due to the large currents that will be drawn from it, as well as the output overshooting possibly. It is imperative that your customer test their final circuit in their system, especially if it does not include soft start.
I'm not sure I would recommend that for TPS54319. You are free to try it though. I would expect erratic start up, with current limit active. I may give it a try tommorow or Monday.