This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27750: The ON resistance of the open drain output circuit of I2C

Part Number: BQ27750


Please tell me about the following items to estimate the margin of I2C communication in my system.

①The ON resistance of the open drain output circuit (transistor) of I2C
 * Iol=3mA

②The variation of the ON resistance
 * For example (± xx%).
③The variation of I2C VOL
 * Iol=3mA
By the way, what is the condition of Vreg> 2.0V?
Is Vreg a voltage other than 1.8V?
* VOL section of “6.25 I2C Interface I / O” on page 11 of the Data sheet.
I look forward to your reply.