Can anyone shed some light on how I might be able to implement in a discrete manner main driving transistor in linear LDOs the common base/gate and common drain/collector or emitter/source circuit used in some LDOs for current sense for current limit? My application is a discrete LDO (as I am a hobbyist I am building it with discrete components).
By the way I think it is usually drawn as a single transistor with (for the case of PNP) one base one emitter and two collectors with the collector on the left usually being the current sense one and the collector on the right being the main power output.
Also is this what a "Kelvin Source" is for?