This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: Pls help to check application for LM5118

Part Number: LM5118

Hi Expert,

Could you help to check LM5118 if could meet design as below:

------------------------------------------

Vin = 18Vdc  to 72V

Vout = 65V

Po= 150W

------------------------------------------

Best Regards,

Mark 

  • Hi Mark,

    Thanks for reaching out and for considering the LM5118 for this application.

    What is the application?

    The LM5118 can meet the specifications however the LM5118 is a non-synchronous converter so the thermal dissipation of the diodes must be considered.

    Please contact me directly if you have any questions.

    -Garrett