This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51220: 12V Output Using TPS51220EVM

Part Number: TPS51220

Team, 

I am trying to validate the TPS51220 which I plan to add to my EVM. I need the device to output 12V and 5V. I cannot get the EVM to output 12V on either channel. For VOUT2, I changed the R21 to a value of 297k ohm, and left R24 at 27k ohm. After populating this resistor, VOUT2 does not output anything, and if I try to repopulate R21 to the original value, it is unable to output 3.3V. I then tried to reprogram VOUT1 to output 12V by changing R2 to 330k ohm, and depopulating R22, but the EVM is still unable to output 12V. Any help would be appreciated.