Other Parts Discussed in Thread: BQ77915
Regarding the BQ77905 and BQ77915
bq77905 datasheet:
“The device's stackable interface provides simple scaling to support battery cell applications from 3 series to 20 series or more.”
“bq77905 supports 3-series-to–5-series cell configuration. Up to four devices can be stacked to support ≥6-series cell configurations, providing protections up to 20-series cell configurations.”
Bq77915 datasheet:
“The BQ77915 device supports 3-series to 5-series cell configurations. Up to four devices can be stacked to support ≥6-series cell configurations, providing protections up to a 20-series cell configuration. It is possible to support greater than 20-series cell configurations, but with careful consideration of delays.”
Do you have any information on how I can safely use these devices with 24 cells? I won’t actually be using the current sense or load detecting features and will likely use the DSG and CHG pins as fault indicators for OV/UV.
Thanks,
Lauren