This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fusion Power Designer parameters not loading

Other Parts Discussed in Thread: TPS53655

I am using the TPS53655 and have loaded it with a project file.  However, there is one strange thing with the power designer software though.  When I load my project file into a device, a few of the settings do not get loaded.  Specifically, the settings that don’t get loaded are:

 

Vin startup voltage

Vin undervoltage

 

And

 

VCCIO/BEN pin setting

 

I have confirmed that the project file has these settings correct, but when I load the file into a device and read them back, they are set at the defaults.  I’m not sure if it’s the way I’m loading the parameters or not.  Any advice T.I. can provide?