This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: over current protection settings

Part Number: BQ77915

Hi:

If I don't need discharge overcurrent detection,How much resistance should OCCP connect?

If I only need battery balance, how do I set it up? 

Thankyou

Regards

  • Hi,

    If you are not interested in current protection, then the BQ7791504 could be a good fit for your application. You would need to short the SRP and SRN pins. The TS pin needs a 10k Ohm resistor connected even if the temperature protection function is not used. VTB can probably just be left floating. Since load removal isn’t required, LD can probably just be tied to ground. All other pins need to be configured according to datasheet recommendations.