This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H000-Q1: alternative solution

Part Number: TPS1H000-Q1

Hi Sir,

My customer is designing a panel system for automotive and need a power input inrush current limit device.

I think TPS1H000-Q1 might be a good fit, but it could not meet customer's requirement.

So I am seeking your help to see if you could advise a better solution for my customer.

Customer spec:

1. Vin(36V max), typical 12V.

2. Current: 4A.

3. When in light load(<0.1mA), the power consumption of TPS1H000-Q1 need to be under 0.04mA.

4. The EN pin of TPS1H000-Q1 need to be 36V supported.

The reason they need a inrush current limit IC is because there are big Caps on their system and they need to limit the inrush current.

Many thanks,

Patrick