Other Parts Discussed in Thread: BQSTUDIO
Hi,
We are trying to use BQ35100 fuel gauge IC in our product to check the remaining percentage of Tadiran TL5930 (19000mAh) battery. Am new to this Power management field. I have below doubts.
1. This battery TL5930 is not listed in the Chemistry IDs. Can we use TL-4930 (1900mAh) ?
2. We calibrated the battery and programmed it with Chemistry ID 0608 of TL-4930. And we configured it into EOS mode. Here we are having few confusions.
a. As per the data sheet SLUSCM6E 8.2.2.2.1.2, it is mentioned that we have to give Gauge_Start() 1s prior to the high load pulse starting in Step 3. Here can I know what is this high load pulsing exactly means ?
b. In the step 4, it is again mentioned that we have to give Gauge_Stop() directly after the high load pulse has stopped. How we will know when it is stopped ?
3. In EOS mode, at what rate we should read the battery percentage. Like every 1 hour or every 24 hours ?
4. In EOS mode, do we need to control the load ? -- In our design, we are using a BLE Module which is having on board i2c interface to which this BQ35100 is connected. So to this battery this BLE module only acts as a load in which our application is running and communication with the BQ35100 is also done by BLE module only.
4. What exactly high load pulsing means ?
5. On turning on the device, can we read the SOH in EOS mode ?
6. With BQ Studio software can we monitor how the Battery is getting consumed by connecting a fixed load to the battery ?