Hi,
Can i able to achieve Vout=+12V with Iout= 150mA atleast, Actually my Load requires 100mA , so for a safer side I was thinking of to have a Source current atleast 30% to 50% more than what the load consumes? Can this be achievable with TPS61093, what could be the effeciency if I operate at 150mA of the system.