Tool/software: Code Composer Studio
Hi,
I'm using EM1402EVM together with LAUNCHXL-TMS57004 and I have some questions about balancing current.
In the EMB1499Q the Absolute Max Rating of VSET are -0.5V to 7.5V and the Operating ratings are 1V to 2.2V. Setting VSET=2V the balancing current are 5A and 3A with VSET=1.2V. Are this the only values I should set VSET? Does the system only work with 3A and 5A? If i want a balancing current of 100mA, can I set VSET=40mV like this or doesn't work like that? Or if i want a balancing current of 3.75A, can VSET be 1.5V?
Thanks.