Other Parts Discussed in Thread: BQ24707
Hello,
I am using bq24715 for a battery charger for a 3S Li-ion battery. It is charger only with no system power output.
Vin and Vcc are 19V. I am not using CMSRC and ACDRV with input FETs, ACOK and ACDET are just pulled up to 3.3V.
This is similar to the circuit I used successfully in the past with bq24707 but in the new circuit I do not see any PWM switching activity.
Charging voltage is set to 12.6V, charging current is set to 1024mA. Cell is pulled up to 3.3V.
I am able to read back from the Charge Option and Minimum System Voltage Registers, so SMBus Comms appear to be OK
The following voltages were observed:
Vin: 19.09V
Vcc: 19.08V
ACDET: 3.29V
REGN: 6.03V
HIDRV: 9.29V
LODRV: 0V
ACOK: 3.3V
BTST: 9.04V
ACN: 19.08V
ACP: 19.08V
SRN: 9.29V
SRP: 9.29V
PHASE: 9.29V
Can you see a reason why the PWM converter would not start up switching?
Thank you,
Carl G.