This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

220V AC in, 24V4A out, Flyback solution with EVM

Hi,

Could you please recommend a EVM which can support 220V AC  in and 24V 4A [normal] out, flyback topology and the most important thing is this solution can offer a EVM which my customer can use to evaluate ASAP.  thanks. 

  • Hello Yue,

    Thank you for your interest in TI flyback controllers.

    The closest readily-available off-line EVM that I could find is the UCC28600EVM evaluation module with output at 19.4V, 6.2A (ref:  ).

    Reference designs that more closely match 24V 4A may be found by searching the TI reference designs starting from the index page (http://www.ti.com/tool/ucc28600evm) but these are not orderable boards.  The selection of orderable EVMs is limited.

    I hope the UCC28600EVM is close enough to be used for performance evaluation.  Obviously, the EVM design can be adjusted "on paper" to the customer's specific requirements, but physically altering the EVM itself may require considerable rework.

    Regards,
    Ulrich