This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using MC34063A for White LED drive of 8 strings of 3 LEDs each with brightness control

Other Parts Discussed in Thread: MC34063A, TPS61165

The topic of using a MC34063A for LED drive has been brought up before.  Certainly, the MC34063A can be used in a boost converter topology to drive a string of White LEDs.

However, if it is possible to implement a brightness control with the MC34063A, how would that be done?  I realize there are other solutions available to do this very thing, but those options have more features than needed.

The particular application will have the following characteristics.

Vin(dc) = 3.3V or 5.2V
Vout(dc) = 9.9V typ and 10.8 max
Iout = 160mA

There is no need to control each string of 3 LEDs individually, but treat the entire assembly as a single string (just know that it is configured as 8 strings of 3 LEDs).