The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM46000-Q1: Problems with proper startup

Part Number: LM46000-Q1

Hi,

I got a problem with the simple switcher LM46000-Q1. When I apply the target input voltage on the Vin pin in one step (0V->24V) the LM46000-Q1 does not work properly. The output voltage reaches only 2V-3V instead of 12V. I'm able to fix that problem by increasing the input voltage in multiple steps (0V->1V->2V->...->24V) but the application doesn't allow this solution.

Do you have any idea to solve this problem?

Kind regards,

Tom