This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160: PMLK using issue

Part Number: TPS54160


Hi,

I meet an issue while using TPS54160 in the PMLK book, related to Ts.

As the datasheet shows: 

Rrt=504kΩ, can calculate fsw=250kHz, Ts=1/fsw=4us. 

But in the experiment, as you can see in the picture, I test the Vsw, figure out that Ts=4.46us, fs=224kHz, which is not aligned with PMLK book.

I think it's caused by these two calculations shown below, but ton min=130ns can't get the 224kHz limit.

Do you have any suggestions?