Other Parts Discussed in Thread: UCC28050
Hello,
I designed a PFC converter which has the following features: Vin = 115V/400Hz, Vout=260V, Poutmax=100W.
The PFC converter goes into overvoltage at startup, the output voltage reaches the internal OVP threshold of the UCC2818 which I fixed at 300V.
I tried to boost the SS capacitor (tried many ceramic capacitor values 100nF, 1µF, 4µ7, 10µ) and it does not resolve the start-up issue.
I tried to clamp the Vaout pin, but the UCC2818 has the same behaviour.
Do you have some recommendations to avoid overvoltage at start-up please?
King regards,