This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: When the UV is trigger, the BQ doesn't goes to ship mode

Part Number: BQ76930

I'm using BQ76930 for BMS. When battery voltage is below undervoltage threshold, the BQ76930 doesn't go to ship mode. I measured on the pin REGOUT which is still 3.3V. The ADC_EN from sys_con1 is set to 1 already. What could be the issue?

Thank you.