Part Number: TPS2663
the pins 19-24 of TPS26633 (VQFN) are indicated as 'not connected'. They're supposed to be used for cooling the device. But are there any restriction, related to the voltage which may be applied to that n.c. pins?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2663
the pins 19-24 of TPS26633 (VQFN) are indicated as 'not connected'. They're supposed to be used for cooling the device. But are there any restriction, related to the voltage which may be applied to that n.c. pins?
Hello Hanno,
There is no restriction on voltage for NC pins. These can be connected to IN or OUT pins up-to operating voltage[60V] of the device.