This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV767: looking for LDO with input max to 24V

Part Number: TLV767
Other Parts Discussed in Thread: TPS709

Hi Champions,

I'm looking for a LDO with the similar performance with TLV767, my request are

VIN MAX: 24V

Accuracy < +/- 1%

VOUT: 3.3V

Iout: 100mA

package less than 3mm*3mm

I see the TVL767 is very good performance, but the input voltage max is only 16V, do you have any other chip suggestions?

TLV767 16 +/- 0.5% 1000 2-mm × 2-mm WSON