This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R3-DEVICE-FW: Maximum Turbo Current Can't reach setting value

Part Number: BQ40Z50-R3-DEVICE-FW

Hi,

I'm using bq40z50-R3 and set Design Capacity to 8200 mAh, then I set Turbo Cfg: Ten Millisecond MAX C Rate to -4.0 C.

but when I Read the Maximum Turbo Current, it's only show -26319 mA, doesn't reach the setting value, does any anther setting will limit the Maximum Turbo Current?

Thank you.

  • Hi,

         bq40z50 would calculate the MPPC based on Rhf, Reff, Pack Resistance and System Resistance and the present DOD of the pack, once the calculated value is less than -0.4C, it will adopt the calculated value instead of the Max MPPC value stored in dataflash