I am using uc3843a in my flyback converter.
for now, I'm giving supply to ic with potential divider from the supply of 50 volts which is also input to the flyback.
the converter is working but voltage to Vcc is dropping down to around 8.4 volts which is making it start for some time then stoping it, I will attach a photo of this happening which contains Vcc volts and gate to source volts.