Hi all,
In DRA72x EVM, TPS65917-Q1 part is PO917A13DTRGZRQ1, which according to https://e2e.ti.com/support/legacy_forums/automotive/f/26/t/563795?tisearch=e2e-sitesearch&keymatch=PO917A13DTRGZRQ1, it means:
- TPS65917-Q1
- 1.1
- OTP = 3D
The problem is OTP=3D is NOT selectable in the TPS65917-Q1 "Order Now" section and it is NOT listed in the "TPS65917-Q1 User’s Guide to Power DRA7xx" OTP versions list. In the mentioned list, compatible OTP versions are:
So the questions are:
- Does the highlighted phrase means PO917A13DTRGZRQ1 OTP version 3D is equivalent to OTP versions 30/31?
- If the answer is YES, then Which one is the behaviour off GPIO_6 in the DRA72x EVM design? POWERGOOD? NSLEEP?
- If the answer is NO, then What OTP version should be chosen to match DRA72x EVM design?
Thank you very much in advance,
Regards.